I am using a bq24090 to charge a battery and power the system.
Currently I have TS floating, with the ability to pull it down via
- bq27510-g2 BAT_GD output (as required for obtaining the OSV measurment for the fuel gauge)
- a host processor via open drain mosfet
The system load is typically light 40mA but can peak at over 500mA.
Charging current is set at 100mA normal with ability for the host to pull ISET2 to gnd boosting it to 500mA.
Temeperature monitoring is being done using the bq27510-g2's internal sensor and as the fule gauge is talking to the host charge control can be transferred to the fule gauge/host.
My question is should I be using TTDM mode or should I connect a 10k resistor from TS to gnd and use the normal mode (with no temp sensing)?
Thank you