This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24735EVM



Hi

Our customer got a EVM board and checked.
VCC=19.5V,DCIN=19.5V

ACDET=19.5V
ACOK=2.6V
SYS=19.5V
REGN=6V

but ACDRV=25.7V and CMSRC=19.5V.
BAT=3.13V(not connect battery)
The ACDRV,CMSRC=6V and BAT=2V written in the sluu507a User's manual.

And Charge Option(0x12H) register's default is F912H.
This manual is F902H. 

Is not this board working?

Regards,
PAN-M