Hi All,
I notice that the Rds(on) of the switch for the TPS61042 does not seem to come into the equations for calculating minimum load current (other than to effect the efficiency). It would seem to me that this would have a significant effect at low voltages, for example an Rds(on) of 2 ohms would introduce a voltage drop of 1V at 500mA so that the voltage across the inductor when current is ramping up would be less, and Rds(on) may well be higher than the quoted 2 ohms at low voltage.
My question is this: Do the conditions that cause Rds(on) to increase towards its maximum also cause the peak current value to increase towards its maximum? Rds(on) increasing would effectively slow the switching frequency, and hence tend to reduce the max power that can be transferred into the output, but if Ipeak increased proportionally then the energy transferred per cycle would increase to compensate.
In other words, can I neglect the Rds(on) value and simply use the Ipeak(min) value of 400mA in my calculations and an efficency of 70% when calculating the load current at minimum input voltage?
Thanks!
Mark.