I'm designing a variable output dc to dc converter with vout anywhere from 5 to 24 with a 2A limit. Vin 5 to 34 volts. I'd like ss, uvlo, and some kind of short circuit protection, ovlo would be nice but not required I was looking at the LM25118, but I also need two control inputs, one is basically a voltage or current input into the converter that can vary the output and the second is a resistance pot that is used to initially set the default output. Any ideas for a controller.
Thanks for all your help.