This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't generate .senc file for bq3050

I cannot download a .senc file from my device. 

I'm running version 0.9.90 of bq eval software.  I have programmed the device using a .senc file with the correct chemistry ID, then loaded in my GG file to configure dataflash.  I issue the 0F00 command to put the device in ROM mode.  When I try to download to a .senc file, I get the following error.

Error in reading flash!  VB_BAD_CRC Flash contents may be incomplete!

I have tried 2 computers and 2 EV2300 modules and get the same error.  I also tried reprogramming with the default .senc file and still get the same error when downloading.