This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54325 TA vs Output current Data

Genius 4220 points
Other Parts Discussed in Thread: TPS54525, TPS54325

Hi,

Does anyone have the "OUTPUT CURRENT vs AMBIENT TEMPERATURE" graph

same as in TPS54525 D/S page12 figure13 ?

If not, Would it be possible to make the graph for TPS54325?

Thanks

Go

  • For TPS54325, the graph is not needed.  TPS54325 can support 3 A output for the entire operating ambient temperature range of -40 to +85 C on a well designed pcb.  So essentially the graph would just be a straight line at 3 A.

  • Hi, John

    Thank you for your comment.

    I tried doing the WEBENCH simulation for TPS54325 under the following conditions.

    (Vin=12V , Vout=3.3V , Iout =3A , TA=85℃)

    but I couldn't do that due to the over junction temp. 

    In TPS54325 D/S, THETA-ja=55.6℃/W with High-K board.

    so we need over 90% efficiency under the condition that described above.

    Is it really possible to support 3A output current for a general assumed conditions like that?

    Thanks

    Go

  • can you post your exact inputs to webench?  I'll see if I can duplicate it.

  • Hi, John

    Here is the info about WEBENCH simulation that I did.

    please see the attached file.

    Thanks

    Go 

    Webench Simulation result.pptx
  • I'll see what i can find out.  it may take a few days.

  • I checked this circuit on the bench.  To summarize the webench results:

    Theta JA = 55.6 C/W (JEDEC standard coupon)

    Pdiss = 1.34 W

    Ta = 30 C

    Tj = 30 + 1.34 * 55.6 = 104.5 (webench actually calculated 105.6 C, probably some rounding error)

    Bench result, Vin = 11.98 V, Iin = 0.956 , Vout = 3.327 V, Iout = 3.00 A

    T top of case = 52 C.

    Ta = 25 C

    Pdiss (minus inductor conduction loss) = 1.3 W (pretty close to the calculated webench Pdiss1.34 W)

    Tj = Tc + psi JT*Pdiss = 52 + 1.8 * 1.3 = 54.34C.

    T rise = 54.34- 25 = 29.34

    Theta JA for EVM = 22.57 C/W

    So the actual EVM thermal performance is better than 2 x the JEDEC coupon.  JEDEC coupon results are really more for comparison purposes rather than actual results.  It allows devices to be compared using identical standard conditions.  For a well designed PCB, the TPS54325 should be able to deliver full output up to Ta = 102.4 C, well above the recommended operating temp of 85 C