Hi, I am looking at page 5 of the data sheet for the bq29200 voltage protection and cell balancer and I see the equations for the cell balancing current (ICB1 and ICB2) but cannot figure out where in the table above showing the recommended cell balancing configurations the calculated values of the cell balancing input current come from (for example the 5,10, 15 mA for the 120 Ohm RCB test condition). Can you explain how the equations for ICB1 and ICB2 relate to the values calculated in the table for ICB or how those values were calculated?
Thanks, Tim