LM5118 power up under load not possible - stable operating point is not reached
I've a LM5118 design which works properly if the load is switched on after power up. But if the load is on during power up the output voltage do not reach stable operating Point - the output is ringing.
With lower load during power up it works but not with higher one.
I've checked the design with WEBENCH - the part which I have used match to the suggested part from WEBENCH.
I've tried several changes on the compensation network - unfortunately with no success.
My special question: which parts of the compensation network impact the stability during power up?
Thanks for any hint that can help me to find a way out...
Walter