Hi,
I've some questions regarding reverse current protection circuit in load switch.
I need to put a regulator circuit for HDMI source, +5V. Normally, I use an IC protection like TPS12S016 which has integrated back-drive protection where it protect a case where user plug the source device to another HDMI source device either it has power or not.
- Does the reverse current protection circuit in this load switch or in some serie of LDO like TPS709xx serie has similar feature to the back-drive protection circuit found in HDMI protection device mentioned?
- Can it protect the case where Vout is supply with voltage while there's no input voltage?
Thanks,
Pornchai