This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63001 Getting hot and consuming power... Why?

Other Parts Discussed in Thread: TPS63001, TPS63000

Dear fellow engineers

I am experiencing a problem with a TPS63001 getting hot (like 60 deg Celcius) and consuming a lot of power (300mA @ 4,1V), yet the output voltage is regulated perfectly to 3,3v. I have found this blog post explaining exactly the same problem though with a TPS63000. Unfortunately the blog ends with a private email exchange, thus no solution published.

In my case I have designed the following schematic:

DC/DC Converter Details:

V_IN = 2,9V -> 4,2V (3,7V LiPo Cell)
V_OUT = 3,3V
C_IN = 10uF X7R
C_OUT = 2x 10uF X7R
L = 2,2uH, 1,5A, 87 mOhm

...with a battery voltage monitor to avoid deep discharge and a main switch. PCB Layout:for the DC/DC converter looks like this:

I have measured the current consumption on the battery supply line, the 3,3V output line, the control-circuit input lines and inductor for no-load and 120mA load:

V_IN=4,1V No load 120mA load
Battery Supply 300mA 420mA
3,3V Supply Output  - 120mA
Control logic * *
Inductor output 20mA 130mA

* This value is so low that I could not measure it

I can not see any other reason to this problem that the chip is broken, but I am not sure why this has happened. In the referenced blog post it is suggested that a start-up voltage peak in the inductor can damage the DC/DC Converter, but I have not yet been able to measure if my system is exposed to this kind of voltage peak.

If anyone have a suggestion to why this chip consumes so much power, and a suggestion to how I can prevent this to happen I would be very pleased.