I am using a TFT display that has the LED backlight built into it (3 Parallel strings of 5 LEDs) . Unfortunately the manufacture tied all of the strings together and I only have access to the a single + and - supply leads. The baclklight requires 60mA at 19.2V.
Will the lm3532 allow me to combine all three sinks together so that I can sink the 60mA. The datasheet doesn't specify if this is a valid use of the device. I would assume if it is possible to parallel the current sinks then one could sink ~90mA by tying all 3 sinks togather?
If the pins can be paralleled to allow a higher current sink, would the max current setting (for my application) in the current register be 60mA/3 (20mA)
Thanks.