Hello Tiers,
please help the analog power supply design in LM5116 here attached my schematic.i did not get constant output voltage.
In output side without load i get only 4VDC and i connect 1K RESISTOR load on out side i get 10V pulsed dc this is not constant one.This voltage is continious
i try this input voltage 30V but in practical application i use up to 20V to 100V /1Amps .
waiting for your valuable suggestions,
5238.DC_DC_100V_V01(GENESIS 200013)_schematic.pdf
regards,
syed