Dear all,
I attached a schematics of a PCB we made recently.
this sch has 2 tiers.
first tier is stepping up (TPS4361) inputs from 12V to 23V to 25V, and second tier is a charger (BQ24610), which charges in 21.5V.
1st Tier:
only stepping up 20V and up to 25V. when you lower the voltage, the output voltage goes down as well.
2nd Tier:
I'm checking the output with no battery, and I get 1.2V on the output.
I can measure 1.6V on TS pin, so this is not a bad NTC problem.
I applied 24V on Cin (C7,C8), to isolate the step up influence, and still, no output.
please tell me if anymore measurements and data are needed.
any suggestions?
best regards,