I hope you can help with the bq27410EVAL I have. I'm trying to upgrade the EVAL board from V1.01 to V1.03 and have the bqSWEV program installed. However the default dfi file in the sw install is V1.01, while the senc file from the bq27410 folder is V1.03 and I can't find any mention anywhere of how to program the senc. I have used several of the bq20zxx which seem to be better supported, at least you can usually find an answer in the documentation.