This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61220 current output problem

Other Parts Discussed in Thread: TPS61020, TPS61222, TPS61220

Hi sir,

          i had designed the boost converter for 2.8V output for 1.7V input , by component values R1 =1.7M, R2=370k,

l=4.7uH,C1=10 uF, C 2=10uF

the boost converter was working  good ,

then i loaded a 10 ohm resistance at output  (2.8 V), so the output current will be 280 mA.

but when we connected the load 10 ohm the output voltage was dropped to 0.6V

we need output current 280 mA for 10 ohm resistance

how do i can get it?

please guide me

Thank you 

Regards 

Rajesh