Hi,
I would like to use use two LP38798 regulators in parallel to increase the output current. The regulators are going to be used as post regulators for a low noise linear PSU for an audio application.
Is if it is possible to use the regulators in parallel and does it effect the output noise?
If the regulators can be used in parallel what would be the best electronic circuit to achieve this. My goal is to get a minimum output current of 1250mA, lowest possible output noise and the output has to be adjustable to 5/9/12/15/18V.
Uin = Uout +0.7V
Ccp = 10nF NP0
Cin = Os-Con 20V - 120uF 25mOhm + 10uF X7R (for each LDO)
Cout = OS-Con 20V-120uF 25mOhm + ??????
Regards, Wiebren