Hello, I am looking to design a control system to automate a material testing rig (see below).
...A motor will be attached to the screw on the right side of the machine, and turn to fatigue the sample placed on the left. I am looking to power this system using a 24 V DC motor (see below). The system will be controlled using National Instruments Lab view software and an output module ( NI9263 - that supplies 10 V (@1 mA).
Link to power module: http://sine.ni.com/nips/cds/view/p/lang/en/nid/208806
Link to motor spec: http://www.parttarget.com/3010-01-056-9045_3010010569045_5A3128.html/-9F8AB34A-C927-4B8B-AB52-88B498E975AB
The output module provides power at only 10 V and I am looking for a system that can boast that to 24 V. I ultimately will create a program using a PWM signal that can modulate the speed of the motor, but am having trouble deciding how to get 24 V out of the 10 V module.
Is there a kit that can be purchased for this project, or a circuit I can create to get 24 V in order to operate the motor.