TPS650250 design we are only using LDO1, what is the recommendation for the unused LDO2 output and feedback pin?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TPS650250 design we are only using LDO1, what is the recommendation for the unused LDO2 output and feedback pin?
thanks
Hi Burak,
The TPS650250 does have a global ENABLE pin for LDO1 and LDO2. - You can not enable only LDO1 or LDO2
So e.g. if you are only using LDO1 (LDO2 not needed in the application) LDO2 will still be turned on with LDO1.
In such a scenario I would recommend to connect a small ceramic output capacitor on the not used LDO output to make sure the output is stable.
FB_LDOx can be directly connected to VLDOx - this way you save the external components for the feedback divider.
In case both LDOs are not needed you can hardwire VIN_LDO, VLDO, FB_LDO and ENABLE_LDO to GND.