Hi, I'm looking for 2 dcdc converter solutions. I work for a large automotive electronics manufacturer and we are in the engineering stages for an innovative system architecture for car infotainment. For this project we need 2 dc dc converters with the following specs:
Converter1:
Vin: Car battery 12V
Vout: 6V, current 2.5A
Switching frequency: higher than 2MHz. It might be lower than 2MHz, but then the frequency must be well known or selectable between 2 or more fixed frequencies
Converter2:
Vin: Car battery 12V
Vout: -6V, current 100m
Switching frequency: higher than 2MHz. It might be lower than 2MHz, but then the frequency must be well known or selectable between 2 or more fixed frequencies.
Best regards,
Hans Rosenberg