This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63030 – Feedback Voltage (VFB) at PS/SYNC=VIN , TA= -40℃ to 85℃

Guru 21045 points

Hi,

 

I believe that the feedback voltage(VFB) value of datasheet is the “495mV(min) / 500mV(typ) / 505mV(max)” at PS/SYNC=VIN , TA=25℃.

However, my customer would like to know the VFB value at PS/SYNC=VIN , TA= -40℃ to 85℃.

Please let me know this value (min / max).

 

Regards,

Kanemaru