Hi
We are usingIC BQ24617 as a Battery charger system as defined in the datasheet.
Problem statement:
We observed reset of power supply( O/P of battery chareger ( supply to system) . It is possible to appear this phenomenon the following situations.
> connect AC power(15V) and no connect Li-Ion battery
> main switch ON
> BY heating the neighgorhood area of the battery charger IC
I used a hair dryer to heat the area
Observation;
When we heat the battery charger IC BQ24617 area using the hair drayer we obaserved there is reset at the batteryu chareger o/p. When reset occurs, the temperature ( measured with equipmemt) of the IC1000 surface and the board surface is around 45 degrees.
This temperature is not so high and occurs in normal operation.
Plese help us in this regards