This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65921B power up problem

We are using the TPS65921B companion chip to power an AM3707 device.

We have 4 identical PCBs, 2 operate correctly and 2 are exhibiting similar faults.

Both of the boards are configured in master mode configuration.

Board one has no DC-DC voltage outputs other than 1.8V. There is no 32kHz clock present and VRTC is 0V. SysEn and Warmreset are being pulled low by the device. PwrOn is high (3.3V). SysEn=0.5V. HFCLK out = 0.5V.

Board two has DC-DC 1.8V present and the other 2 supplies attempt to come on and then power off again.  There is a large periodic pulse every 200ms which coincides with the supplies trying to power up. The 32KHz clock is present (0.5VP-P with 0.7V dc level). SysEn and Warmreset are being pulled low by the device. PwrOn is high (3.3V). SysEn=0V! HFCLK out = 0V.

If the 3.3V input supply is lower to 3V and the device powered up the spike is not present.

Thankyou

  • can you please check if there is any kind of short on the board, from what you are explainaning it seems like there is a short and device shuts down because short circuit triggers.

    You can try to remove the laod and see if the board boots up properly.

  • Hello

    Thanks for the response. Yes we have checked for potential short circuits and have compared resistances with a working board. One of our thoughts is whether we have a device population problem and the output sense lines may be open circuit. I will keep you posted.