What is the PMIC quiescent current if the power rail requirements are as such below. In the case shown, the processor is in stand-by and is powered by USB. No specific PMIC has been chosen, but we were looking at the TPS65023, TPS6507x and TPS650250 just to get an idea.
3.3 V Supply | 0.4 mW | 0.121 mA |
1.8 V Supply | 0.25 mW | 0.139 mA |
Core - Fixed | 0.5 mW | 0.5 mA |
Core @ 0.85V | 2 mW | 2.353 mA |
1.8 V Supply (mDDR) | 1 mW | 0.556 mA |
Regards, Andy.