Hi,
For Solar street light applications, I'm using TPS92690. To the
specifications input:12V, Out: 48V, 700mA, I customized the components
value. But when connected to the 2 parallel strings of 12 series leds,
the led tends to flicker and takes just 300mA. I used Radj1= 40K,
Radj2= 100K to set output current to 700mA. Kindly revert the solution
as soon as possible.