Dear Sir
May I know why BQ24751A is not recommend for the new design?
Why recommend to use BQ24725A? What's benefit of BQ24725A and better than BQ24751A
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kai,
A few of the reasons for migrating to the BQ24725A are the following:
-Smaller package migrating to a 20-pin QFN
-Lower Quiescent Currents
-Multiple Switching Frequency options in case certain harmonics must be avoided.
-Higher Switching Frequency resulting in smaller inductor and filtering capacitors.
-Less Expensive
These are just a few of the positive benefits of migrating to the BQ24725A. This is on top of the support available for this active device as compared to a device nor recommended for new designs.