hi, i'm trying to make a 5V 1A flyback supply, usig a coilcraft transformer B0570-BL, http://www.coilcraft.com/ncp101x.cfm.
now, i'm using the standard circuit with Rs1=120k, Rs2= 30k, Rlc=4.7k
my problem is that the output at no load i've 5.5V but when i connect a load the output voltage falls to 0.5V, what can i do? maybe to use a sensing circuit on the output?
thanks