Other Parts Discussed in Thread: TPS60400, LM2664
I am going to possibly use TPS60400 in a design to provide the negative rail to an op amp for a bipolar output. My design is very space sensitive, and I would like to know if the input capacitor is needed if I am feeding the device with a switching power supply. with 10uF and 0.1uF in parallel on the output of the switching power supply. The TPS60400 will be very close to the switching power supply. I plan to use 1uF fly and output caps on the TPS.