Hello
I
am trying to measure the current coming from a RC LiPo charger with the bq34z100evm board.
If I use a stabilized power supply and a Fluke amp-meter and adjust the current to 500mA showing on the amp-meter the bqEVSW software shows 500mA. If I use the RC LiPo charger adjust it to 500mA, the Fluke amp-meter shows 500mA but then the bq34z100evm board reads only about 400mA. If I use the same setting with the LiPo charger on a bq20z45evm board I see 500mA with the bqEVSW software.
Do you have any suggestions why the bq34z100evm reads a 25% smaller current with the RC LiPo charger than with the stabilized power supply.
Regards Fabian