This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54426 - Combining Vreg5 pins of two regulators

We have two such regulators on our board. One drops 12Vdc to 1.8V , the other drops 12Vdc to 2.5V.

EN pins are fed from the same 12V dc source, so, both parts are on.

How can we combine the Vreg5 output pins of the two requlators to obtain 5Vdc at 100mA?