[ LM5088 ] Instability
Hi,
According to my customer, they are seeing the instability which cause Vout is getting half of the target voltage.
Here are the conditions.
---
- LM5088-1
- Fsw 550KHz
- 42Vin
- 8.3Vout/1.5Aout
---
Customer's outcome are...
- When Vin is relatively high such as more than 40V, Vout is getting half.
- When customer connect their probe to FB pin, this can be disappeared.
- When they use 100pF Cff(feed forward C) in parallel with high side feed back resistor, this can be improved.
Still not much information from customer and I'm now working on having more info. and waveforms from customer.
As like other posts, some points I need to check.
- Current limit could be triggered by noise or other causes.
- External compensation is not optimized (their Rcomp and Comp 43Kohm/2.2nF are slightly small compare with Webench design)
- Their Sense resistor (27mohm) is slightly small compare with
Do you have any other ideas where I should look into?
Also, can you please let me know whether Cff work well for ECM type of device?
Thank you for your support in advance.
Regards,
Ken