Hi
Would like to check with you on the soldering profile of this module PTV12010LAH.
Is there any special recommendation on the soldering temperature, solder wire or iron tip for manual soldering this part?
Ivan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ivan:
PTV12010LAH is a vertical through hole power pin module. It can only be wave soldered or manually hand soldered. It is not compatible with surface- mount reflow processes.
It must not be SMT reflow for any reason as the individual components will either become unsoldered, separated from their respective power terminations or fall off the module PCB.
Manual hand soldering pin(lead) temperature is limited to 260°C for no more than 5 seconds.
Tom