Hello TI Gas Gauge experts-
We are using the BQ26925 is a design and would like to take advantage of the open cell detect feature. On page 17 of the data sheet it says "In a normal system, closing a cell balancing FET will cause 2 cell voltages to appear across one cell input." This is up to 8.4V, well in excess of the absolute maximum rating of 6xn at VC1 (6V) given on sheet 4 for cell input range.
What's up with that? It seems like we are exceeding the rating of the device, just like the data sheet tells us to!
Thanks in advance for clearing this up, and Best Regards,
-Tim Starr on behalf of BA@IW