This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61016 with Lithium Iron Disulfide (1.8V) cells?

Other Parts Discussed in Thread: TPS61016, TPS61010

I have a customer that has been using the TPS61016, which has an abs max 3.6V input voltage rating. They use two alkaline batteries.

They want to be able to tell their customers that they can use Lithium Iron Disulfide cells for longer battery life - actually they have already told their customers this.

These are new to me. The marketing blurb for the battery (http://data.energizer.com/PDFs/lithiuml91l92_appman.pdf ) says this:

Although the higher OCV of the LiFeS2 system is 1.8 volts, the nominal or rated voltage is 1.5 volts which

makes it a suitable replacement for alkaline and nickel systems. The battery voltage will drop when it is placed

under load. For this reason, the higher OCV will typically not damage electronic components, but device

designers should take into consideration that the OCV of fresh batteries can range from 1.79 to 1.83V. LiFeS2

batteries fully meet the ANSI specification for a 1.5V battery. When a drain has been applied to the battery,

the OCV drops dramatically and then slowly recovers with time. The OCV for a battery can be misleading. A

“good” battery will generally have an OCV >1.74 volts. Any battery with an OCV <1.70 (after it has been

allowed to recover) is completely discharged. Although an alkaline battery may read “good” at 1.6 volts, this

reading on a LiFeS2 battery indicates the product has been discharged.

Does anyone have experience with these? How much load does it take for the voltage to drop?

Thank you -