I have used the LP8545 on a design and like it. Have a new design where I have two LED strings. The load on each is about 110mA with a voltage of 8.1V to 9.3V. I think i can get there if I load share three current sinks on each string. I don't need I2C but do need a PWM input. Is there another IC that would work better?