Hi,
In the datasheet of TL751L12, Fig 4 shows the stability of the regulator with respect to the ESR of output capacitor.
As per datasheet information the ESR should be less than 0.4 to have a good stability.
But, usually the ESR of capacitor is mentioned at particular frequency. For a ceramic capacitor ESR is mentioned at 100KHz.
My question is as follows;
1. The ESR information given in the Fig 4 of datasheet doesn't have any frequency information.Please let me know the frequency information of ESR, i.e at what frequency the ESR of capacitance should be <0.4 ohm.
2. I have selected T495X106M035ATE250 capacitor as a load capacitor.Please give your comments.
Thanks,
Jebas