This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355 / influence of Vreg voltage

Guru 20090 points
Other Parts Discussed in Thread: TPS53355
Hello,
 
TPS53355 Vreg is 4.27V(min) when Vdd is 4.5V which is minimum recommended voltage.
Are there any influence to operation at this Vreg voltage (or less than 5V)?
 
According to Table 1 and 2, I think that Vreg will impact to the switching frequency and Softstart time.
 
Best Regards,
Ryuji Asaka