Hi, I realized a design with the BQ 24618 coupled with a BQ 29312 and a BQ 2084-V143.
My design is completely functional but the BQ24618 Heats !!! I want to know if it's "normal" because My design is going to be produced something like 500+ pieces
This is my prototype and I have do a mistake. I haven't link the power pad to my ground plane... (I have one on a mid-layer but I remove it for link the different ground at a single point)
If I charge my batteries (2600mAH 4Cells) when I have charged about 25-30%, the charger Stop to charge, wait some times and charge again. (I can't put my finger on it, it's too hot)
My Question is : Is it Normal the BQ24618 is Heating?? I don't understand why he can heats, the current is in the Mosfets...
And if it is normal, is it sufficient put my powerpad to a ground plane (or two)?
Thx