Hello,
I would like to prevent a Short Circuit case as the shown on the follow image using an IC. Ones of my priorities are:
- Maintain low power comsumption. About uA currents.
- When the SC is detected, no damage can´t ocurred, the idea is that once the SC dissapear the circuit continues working fine.
According to the image, GP1VCCOUT is the same VCC voltage which is commuted.
I hope you can help me with this.
Thanks for your attention.
Ricardo