Hello,
I have a problem where the LM2611 inverting Cuk converter is locking up after a short circuit event. After a short, it current-limits the upstream power supply (set to 200mA) and stays that way until it is power-cycled. The circuit I am testing is the TI LM2611 evaluation module board with the 10k feedback resistor replaced with a 20k resistor to give me -3V and the C_cuk replaced with a 100V 1uF capacitor.
The datasheet makes no mention of short circuit protection, is there a way to make this switcher handle short circuits gracefully?