This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100 State of Charge showing wrong

Other Parts Discussed in Thread: BQEVSW, BQ34Z100, BQ34Z110

Hello,

We are using  Li ion 2 cell battery with max 8.4 V and 3400 mAh. In my application minimum battery voltage is 6 V.

So the range is 6V-8.4V. How can I set the limit for minimum and maximum voltage values.  I am reading 0x02/0x03 satate of charge registers, it is showing wrong  % status of charge . But I am getting exact battery voltage while reading 0x08/0x09 registers. How can I configure with the above mentioned range? Please suggest.