Other Parts Discussed in Thread: UCD3138
Hi,after getting the ADC14 value of UCD3138 ,how to convert it to temperature value?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Felix,
Take a look at the Temperature Sensor section under the Electrical Characteristics table of the Datasheet. This gives you the Voltage Resolution (5.9mV/°C). It also shows the temp range is -40°C to 125°C which corresponds to a voltage range of 1.46V to 2.44V. Finally it mentions that there is a factory trimmed 25°C reading that is per device.
Please reference section 4.20, and section 4.23 of the Datasheet, and sections 1.11, 1.12, 2.3, and 2.6 of the Monitoring and Communications Programmer's Manual.
The factory trimmed 25°C reading is in the TEMP_REF register. So get the value in that register and convert it to a voltage: Vtrim = 2.5 * 4096 / TEMP_REF.
Vtrim is the voltage measured for that device at 25°C.
Likewise, take your temperature reading from the device and convert it to a voltage.
From here you can use the straight line formula y = m * x + b, where m is the voltage resolution of 5.9mV/°C, and b is the y-intercept that you can calculate by using the point of Vtrim @ 25°C.
Section 3.8 of the Datasheet describes the devices temperature performance characteristics.
Please let me know if you have any more questions. Thanks!
Regards,
Brandon Vonk
Brandon Vonk,
Thanks for your help and I get the correct temperature now.
I met anther question on my UCD3138HSFB-029 today.The output current of the calculation is wrong,so I want to know about the relationship between the resistance and the temperature of the copper.Can you offer me some information?
Best Regards,
Felix
Felix,
The resistance of this copper trace is close to 0.5 mΩ. However, if you need more accuracy, you should perform a room temperature calibration to measure this resistance more accurately. We usually do this by taking a two point measurement of the output voltage and current, fitting these points to a line and extrapolating the slope (resistance), and the offset from there.
Please let me know if you have any more questions here. Thanks!
Regards,
Brandon Vonk