Hi there.
I have been using the bqeasy wizard v0.9.86 for the bq20z95 and have found strange results for setting the CUV threshold. I am building a three cell pack with LiFePO4 cells and specify 2000mV for the 'minimum rated cell voltage (from the cell data sheet)" and 2167mV for the "minimum cell voltage allowed during discharge (typically this is when your system will no longer function)". This seems to produce the following settings;
CUV threshold 1466mV
CUV recovery 2266mV
Clearly, this does make sense, as the CUV is less than 2000mV - the minimum rated cell voltage.
Putting the bqeasy process aside, I can't seem to manually correct these settings either - when I modify the CUV Threshold 'Value' by typing in a new number and pressing enter on the keyboard, the field turns red and the previous value is reloaded.
I'm sure I'm overlooking something very simple.
Thanks again,
Jeremy.