Hi.
I have simply installed the bq34z100 evaluation SW ("bqEVSW") and the corresponding 32-bit driver for my windows 7 (and resterted my PC). Then I have connected my bq34z100 evaluation module ("bq34z100EVM") through my EV2300. The EV2300 is connected to the bq34z100EVM using I2C (the "mid" EV2300 contact).
Now, I simply want to check if I have installed the "bqEVSW" SW correctly and that the "bqEVSW" have connection to my bq34z100 evaluation module ("bq34z100EVM") through the EV2300. The EV2300 is connected to the bq34z100EVM using I2C (the "mid" EV2300 contact).
But when I launch the "bqEVSW", the following is shown first:
NOTE: It says "AutoDetect device: None" etc.
I then click "Confirm Selection", and the following pop-up appears:
Does this indicates some initial errors (in case what) ?
I hope someone can help me clarifying the situation.
Regards Terje Bohler