Page 7 (LHS) of the following ti.com (below) article is totally wrong, do you agree?
It says that regarding active clamp forward converters, “With sufficiently fast gate drive,
the turn off of Q1 can be virtually lossless.” (Q1 being the main power mosfet).
This is impossible, current cannot suddenly go to zero in Q1 and cannot immediately divert into the clamp capacitor until the drain voltage has risen to V(clamp) + V(diode).
So do you agree that this article is totally wrong in saying that there are no turn off switching losses in the main power fet?
http://www.ti.com/lit/an/snva591/snva591.pdf