This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z90 over current setting enquiry

Hi,

I have a 4s2p battery pack and would like to set its OC Dsg at:

OC Dsg - 40A (1st), 80A (2nd), 120A (3rd)

OC Dsg Time - 100ms (1st), 10ms (2nd) , 100us (3rd)

Is it possible to manipulate the sense resistor to detect the current?

I read the manual and it states the max value is at 20A.

Thank you,

Ken