This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1117IMP-3.3/NOPB LDO Reverse current Protection

Other Parts Discussed in Thread: LM1117, SM74611

We are using LDO: LM1117IMP-3.3/NOPB (SOT-223 package) for +5V input to +3.3V output voltage.

We have also has the +3.3V battery backup at the output of LDO (LDO output pin and battery +ve pins are shorted).

Whenever Input signal is not available to LDO, the batter will supply power to our circuit.

Now our question is, Whether the LDO can withstand a battery voltage at LDO output pin while the LDO input is left open circuit.


I have seen the datasheet of Linear Technology LDO: LT1764 datasheet at page No: 14, They have clearly mentioned in 7th paragraph and given the LDO sink current in Figure 5. The LT1764-3.3 can sink 0.7mA reverse O/P current at battery O/P voltage at +3.3V.


But we are unable to find these Reverse current Protection of above LDO in the datasheet.

So kindly conform the Reverse current protection capability of  LDO : LM1117IMP-3.3/NOPB


Regards,

Sugumar K

India

  • Hi,

    Please see Protection Diodes section of the datasheet. It explains how much reverse current the internal diode can handle inside the LM1117.

    If the input is truly open, then I do not see any issues since no current will be flowing from output to input. If you have an input capacitor, then a quick transient at the output can cause a reverse surge current which may potentially damage the internal diode if large enough. You may place a protection doide between the output and input pins to divert current from the internal diode in case this happens.

    Have you also taken a look at ORing the two supplies? SM74611 might be a good fit here, acting as a very low drop diode (~26mV).

    Tim