This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2676-ADJ Problems



Hello:

I'm designing a 15V and 3.3V SMPS using the LM2676-ADJ. I'm using the evaluation board with the recommended components from the data sheet. The 15V version exhibits a 200mV p-p sawtooth wave @ 400 Hz with light loads and poor load step response. The 3.3v version exhibits an odd pulse-type waveform @ 10 kHz on the output when loaded at 0.5A when the input voltage is raised above 14V and also shows poor load step responds. Please help.

-Chris