Hi All,
I promoted TPS54560 to customer and their requirement is i/p voltage should be upto 50VDC and o/p voltage is 42.40 volts with 5A current. There is one evaluation module available for above part, but it is rated for 5V,5A only.
SO there is bit confusion will the TPS54560 regulator works continuosly for above operation, when we calculate the o/p watts it is close to 210Watts or is there any regulator from TI which is best suited for their requirement at low cost.
Kindly need help on the above.
Regards,
Aravind