Hi,
I would like to use the TPS7A8300 in my new design, I just like to be sure that I will get the lowest drop out voltage possible. The specification indicates that the DOV of this part at 2A is 200mV when Vin > 1.4V, Vbias=open; and DOV=125mV when Vin=1.1, Vbias=5V. From these figures, it seems that the lowest DOV is achieved by having high Vbias.
How can I be sure that I will get the lowest DOV? I can always make the Vbias=5V, but the input voltage varies between 2 and 3.3V, how can I ensure that this part will use the Vbias for the charge pump and not the input 3.3V? What control the switch for the charge pump?
Thanks
Hue