Hi,
I am using BQ24074 IC for charging a single li-ion battery. The battery has no over-discharge protection. On BQ24074 datasheet, there is no clear explanation for the disconnection of battery from the load, in low battery condition. There is BQ24075 chip to do that combined with SYSOFF pin. But this IC delivers 5.5V Vout instead of 4.4V.
Does BQ24074 disconnect the battery from the output in low battery condition? (Q2 off) Do you have any chip succession that has such a functionality, similar to BQ24074?
Thanks and Best regards,
Ismail